Expertise
Value of Bearing Repair for Global Equipment Operators
Deep Repair Expertise
In today’s competitive global economy, industrial companies are always looking to optimize supply chains, manage costs and use resources efficiently. Many turn to bearing repair as a smart, sustainable alternative to buying new.
Jay Alexander, business manager at Timken Power Systems, explains how Timken bearing repair and reconditioning solutions help customers extend bearing life for greater operational efficiency and sustainability.
“We’ve repaired many bearings multiple times over decades and extended their service life by another 50+ years. That’s real value — the kind that keeps our customers competitive and our businesses growing together.”
Jay Alexander, business manager, Timken Power Systems
Solving complexity with capability
From energy and steel production to rail transportation and infrastructure, most highly engineered industrial bearings can operate reliably for a decade or more with proper routine maintenance. Once they reach the end of their planned lifecycles, replacing them can be complicated by factors like tight budgets and lead times for new bearings.
Occasionally, bearings that have operated for even longer may be difficult to replace without reverse engineering to design a new replacement.
Repair is an alternative that helps industrial equipment operators stay competitive. Timken’s capabilities in industrial bearing repair and reconditioning connect customers with service levels tailored to their needs, from minor bearing cleaning and inspection to complete bearing overhauls. According to Alexander, Timken is well-suited to bearing repair due to its engineering rigor and vertical integration.
“When remanufacturing a bearing, we’re taking it through similar processes we use to manufacture new bearing solutions — using state-of-the-art machine tools, gauging and quality standards not available through most machine shops,” he said. “Customers get back a warranted repair from a global bearing leader.”
Also unique: Timken repair operations support most global bearing brands, not just Timken®.
Timken® Bearing Repair Services
Reduce Costs. Improve Performance and Sustainability.
|
TYPE 1
|
Re-Certify | Bearing assemblies cleaned, examined, measured for verification of internal clearances, inspected, preserved and packaged. |
|
TYPE 2
|
Recondition | Bearing assemblies cleaned, examined, polished, honed or tumbled to remove minor surface defects (primarily rust or corrosion), measured for verification of internal clearances, inspected, preserved, and packaged. |
|
TYPE 3
|
Remanufacture | Bearing assemblies cleaned, examined, raceways reground, new roller sets and major components manufactured and replaced as required, internal clearances reset, inspected, preserved and packaged. |
Adapting to changing application requirements
Timken industrial bearing repair solutions are especially vital in industries where uptime is crucial. In addition to reducing lead times by about half, choosing repair gives customers access to engineering and manufacturing expertise.
“We often help modify bearings for new performance requirements by adjusting internal clearances, adding coatings or changing materials,” Alexander said. “This helps customers make use of obsolete inventory they already have on hand or solve specific performance problems that arise.”
For instance, an aluminum producer that supplies automakers with material for auto body panels received complaints about visible waves in the panels once they were painted. Timken engineers suggested design upgrades to the existing bearings to help eliminate vibration issues in the aluminum making process. One factor was modifying the bearings’ vibration coefficient, which was handled through precision grinding by Timken repair and remanufacturing experts. This quickly solved the problem and helped the aluminum producer and its automotive customers back on schedule.
In another example, Timken remanufactured 70-year-old bearings for a movable bridge in the Northeastern U.S. Originally made by Timken, the bearings were no longer replaceable through standard production. Company experts rebuilt the 16 original bearings, applying upgraded internal geometries, to meet the 20th-centruy bridge’s 21st-century requirements.
Adding value through innovation, sustainability and expertise
Being in the unique position of seeing thousands of bearings at the end of their initial life cycles, the Timken bearing repair team shares its findings with Timken R&D and engineering experts. When systemic issues are identified — such as flaws in competitor designs or recurring wear patterns — they use that information to develop new solutions and design options for customers who buy new.
And while lower costs and shorter lead times typically drive customer purchasing decisions, bearing repair also helps customers reduce waste and their environmental footprint throughout their supply chain and equipment lifecycle. Repair and remanufacturing avoid scrap, extend product life and reduce energy use by reusing critical bearing components. By reusing races and other components, they can avoid much of the energy required to produce a new bearing.
When it comes to delivery, Timken industrial bearing repair is often better-equipped to maintain on-time delivery due to efficient processes, broad manufacturing capabilities in its repair operations, and a highly skilled, cross-trained workforce that, like Alexander, have worked at Timken long enough to see specific bearings through multiple lifecycles.
“We’ve repaired many bearings multiple times over decades and extended their service life by another 50+ years,” he said. “That’s real value — the kind that keeps our customers competitive and our businesses growing together.”
Deep Timken expertise in bearing inspection, repair and remanufacturing helps customer advance equipment life and performance across industries. Learn how company repair experts keep essential aircraft flying and help rail operators limit their costs and environmental footprint.
Last Updated: 2025/06/26
Published: 2025/05/29