轴承制造专业术语 

A | B | C | D | E | F | G | H | I | J | K | L | M | N | O | P | Q | R | S | T | U | V | W | X | Y | Z

-----

A 返回顶部

-----


ABRASIVE BLASTING: Process for removing scale from product after heat treatment and prior to grinding; product pieces are placed in a tumbler that bombards the surface with high velocity metal shot particles. This process also acts as a tempering or stabilizing process. (Also called Shotblasting)
磨料喷砂法:热处理之后磨削之前去除产品表面氧化皮的工序;把工件放进滚筒里,用高速金属磨料喷击表面。这道工序也起到回火或退火处理的作用。(也叫喷丸处理)

 

ABRASIVE WEARING: Damage to bearing parts caused by fine foreign particles which get in through badly worn or defective seal and/or lubricants.
磨料磨损:由于密封磨损或损坏以及润滑剂失效而导致外界细小磨粒进入轴承内部从而引起轴承部件的损伤。


ACCIDENT: The occurrence in a sequence of events that usually produces unintended injury, death, or property damage.
意外事故:在一系列的事件当中发生的产品意外伤害、毁坏或者功能损失。


ACID ETCH: The process of checking surface of ground product for cracks or burns by use of a series of acids or neutralizers. Also called Nital Etch
酸蚀:指使用一系列的酸或者中和剂来检查研磨产品表面裂纹或者烧伤的工序。也叫酸洗。


ACME SCREW MACHINE: (See: Automatic Screw Machine )
ACME 冲切机:(参考:自动冲切机)


ADDITIVE: A chemical added in small quantities to cutting fluids to impart certain properties.
添加剂:一种化学品,少量增加到切削液中以影响切削液的某些特性。


AGING: The process of running product through low temperature air draw furnaces for the purpose of relieving stress which was caused in the hardening operation. The process stabilizes the microstructure of the product so it will retain desired dimensions during use. Also called tempering or drawing.
时效处理:指让产品通过低温通风炉以释放淬火造成的应力的工艺。这道工艺可以稳定产品的内部微观结构,在实际工作中能保持产品的尺寸稳定性。也称为回火。


AIR COOL: To cool by passing air over, into, around or through; cooling hot product to room temperature using air as a quenching medium.
空气冷却:用空气作为冷却介质,通过空气使高温的产品冷却到室温。


ALL PURPOSE BEARING: The Timken Company "AP" Bearing; a self-contained pre-assembled, pre-adjusted, pre-lubricated, completely sealed unit. Applied to and removed from an axle without exposing the bearing elements, seal or lubricant to contamination or damage.

多功能轴承:Timken 公司“AP”轴承,是一种成套的预装配、预调整、预润滑、完全密封的轴承,在轴承安装和拆卸过程中避免了轴承部件、密封或润滑油的污染或者损坏。


ALLOY: A substance with metallic properties composed of two or more chemical elements at least one of which is metal.
合金:由一种金属跟另一种或几种金属或非金属所组成的具有金属特性的物质。

 

ALLOY STEEL: A steel containing iron and carbide plus one or more other metals such as nickel, chromium, or molybdenum. The Timken Company is a world leader in the production of high quality alloy steel.
合金钢:指钢中含有铁,碳,以及镍、铬、钼等一种或多种其他的合金元素。Timken 公司是全球领先的高质量合金钢的生产商。


AMERICAN NATIONAL STANDARDS INSTITUTE - ANSI: An agency that develops standards and requirements regarding all things which affect the health and safety of associates.
美国国家标准协会:开发制定影响会员健康和安全的相关标准和需求的一个机构。


ANNEAL: Process of heating metal to a given temperature and then controlling the cooling of same metal so the product is softened properly for machining. (See: 80% Anneal )

退火:金属热处理的一道工序, 将金属加热到特定的温度后冷却并控制冷却的速度,以达到软化效果提高金属可加工性。(参考:80%退火)

 

80% ANNEAL: Tempering operation; process of heating product to remove hydrogen from railroad product so the product does not crack.
80% 退火:回火操作;加热去氢以达到用于铁路的产品不易碎裂的目的。
 

ANTI-FRICTION BEARING: All roller bearings are anti-friction devices; designed to prevent or minimize friction in machine operations through the use of rolling contact. If friction is not minimized, excessive heat and wear will severely limit the life and usefulness of machines.
抗磨轴承:所有的滚动轴承都是抗磨轴承,通过滚动接触设计来防止或减少工作时产生的摩擦。过多的摩擦会产生过多的热量和磨损,从而严重限制机器的寿命和性能。

 

ANVIL: A small piece of ground and lapped steel attached to the frame of a micrometer; serves as a flat, fixed point from which measurements can be taken.
铁砧:一小块经过研磨和抛光的铁块,附于千分尺上面作为平直固定的测量参考点。

 

APEX: The common point on the axis of a bearing where angular lines of each of the various tapered roller surfaces meet.
顶点:轴承中心线和圆锥轴承滚子表面延长线的交点。

 

APICES: Plural of Apex.
顶点:APICES 是Apex 的复数形式。

 

AP BEARING: (See: All Purpose Bearing )
多功能轴承:(参考All Purpose Bearing)

 

ASSEMBLED BEARING: A complete bearing assembly consisting of four basic component parts, the outer race (cup), the inner race (cone), the tapered rollers and the spacer-retainer for the rollers (cage). The "AP" Bearing also contains a spacer, seal, seal wear rings, axle end cap, cap screws, locking plate and backing ring.
成套轴承:完整的轴承套件包括四个轴承基本部件,外圈、内圈、圆锥滚子和保持架。AP 轴承还集成了隔圈、密封、密封耐磨环、轴端盖、端盖螺钉、锁定板以及后挡环等部件。

 

ASSEMBLY DEPARTMENT: Final Assembly and Inspect Department which takes finished bearing components (cones, rollers, and cages) and assembles and inspects them for final shipment to the customer.
装配部门:指最终装配和检验部门,负责检验和装配轴承部件(内外圈、滚子和保持架),以备最后发货给客户。

 

ATMOSPHERE: Elements that make up the air in a confined locality such as in a furnace.
气体环境: 一个有限的空间如熔炉里的空气的组成成分。

 

ATMOSPHERE CONTROLLED FURNACE: Furnace which uses endothermic base atmosphere which is formed by the partial reaction of a mixture of fuel, gas, and air in an externally heated, catalyst-filled chamber.
可控气体炉:一种使用由混合燃料、燃气或者空气在外部加热的催化室里部分燃烧所产生的吸热性基础气体的熔炉。

 

AUSTENITE: High- temperature, solid form of steel; the non-magnetic form of iron; has the power to dissolve carbon and alloying elements.
奥氏体:一种高温的钢的固溶体,不具有铁磁性,可与碳和合金元素溶合。

 

AUTOMATIC SCREW MACHINE: A Machine into which seamless steel tubing is fed onto spindles; a piece of product (cup or cone) is cut off each time the machine completes a cycle. Steel is either turned or formed via carbide tooling into a cup or cone. Also called Acme Screw Machine; manufactured by the National Acme Company.
自动冲切机:无缝钢管在主轴上进给,自动冲切机一次循环可以冲切一块工件(外圈或者内圈)。它是用硬质合金刀具以旋转或者成形的方法把钢管加工成外圈或者内圈的。也称为Acme Screw Machine,由National Acme 公司生产。

 

AXIS: A straight line about which an object rotates; a straight line about which the parts of a bearing are regularly arranged. The center line of a shaft serves as an axis for a bearing; the cup and housing remain stationary while the shaft and cone rotate OR the cone and shaft remain stationary and the cup and housing rotate around it. The relative motion of the cup and cone is accommodated by the rolling motion of the rollers.
轴线:物体围绕着其旋转的一条直线;轴承部件围绕着其均匀布置的一条直线。轴的中心线当作轴承的轴线;轴承外圈和轴承座静止不动而轴和内圈围绕着轴的中心线旋转,或者轴承内圈和轴静止不动而外圈和轴承座围绕着轴的中心线旋转。轴承内圈和外圈的相对运动通过滚子的滚动实现。

 

AXLE: Rod or spindle on, or with which a wheel revolves; the bar connecting two opposite wheels. The shaft, (axle) of an automobile fits through the bore of a cone of the tapered roller bearing.

轮轴:指带轮子可以旋转的杆或轴;或指两端分别连接两个相对放置的转轮的横轴。汽车的轮轴与圆锥滚子轴承的内圈配合在一起。


AXLE END CAP: Cast iron part used to lock a Timken Company railroad bearing assembly onto the end of a chassis (axle); not produced by The Timken Company, purchased from several other companies for use with The Timken Company railroad bearing assemblies.
轴端盖:一种铸铁零件,用来锁紧Timken 公司的铁路专用轴承到轴端上;这种零件并非Timken 公司生产,而是从其他的一些公司采购,用于装配Timken 公司铁路专用轴承。

 

-----

B 返回顶部

-----


BACK FACE-CONE
: The heavy or large outer diameter end of a cone; the wide end of a cone. With exception of unit cone.

内圈大端面:内圈中较厚或内圈外径较大的那一端面;或内圈中较宽的那一端面。多列成套内圈没有大端面之说。


BACK FACE-CUP: The heavy end of the cup; the back face fits against the back housing when the bearing is installed for use.
外圈大端面:外圈中较厚的那一端面;或安装轴承时,与轴承座肩接触的那一端面。


BACK FACE RADIUS: The radiused surface at the intersection of the back face and the inner diameter of cone and outer diameter of cup.
端面倒角:轴承大端面与内圈内径或外圈外径相交处的圆形表面。


BACKING PLATE: Piece of tooling that attaches to the workhead of a machine which supports the product to be ground.
支撑板: 安装于机器工件座的一块工装板,用来支撑待磨工件。


BAD CHAMFER: Chamfer that is eccentric, nicked, torn and/or undersized and which is either scrap or repair.
不良倒角:指偏心的、有刻痕或擦痕,或者尺寸偏小的倒角,这种倒角要么报废要么需要修补。


BAR: Term used interchangeably with tubing or steel tubing.
钢管(棒):有时与tubing、steel tubing 同样表示钢管。


BATCH: (See: Economic Lot Size )
:(参考:Economic Lot Size)


BATCH PROCESS: A method of processing or production in which large quantities of material, information or goods are accumulated and then processed to completion as a unit. Such a process is used, for example, in the manufacturing of a variety of chemical products. (See: Continuous Process)
批处理:指将大量的材料、信息或货物先堆聚,然后作为一批次统一处理的一种工艺或者生产方法。
例如,这种工艺可以应用在生产品种很多的化学产品的场合。(参考: Continuous Process)


BEARING: Part of a machine on which another part revolves, slides, etc. Types of bearings include:

Tapered Bearings, Ball Bearings, Sleeve Bearings, Air Bearings, etc.
轴承:轴承是支撑其他元件并允许其旋转、滑动的机械零件。轴承的类型包括:圆锥滚子轴承,球轴承,滑动轴承,空气轴承等。


BEARING STAND: (See: Stand)
轴承标准:(参考:Stand)


BEVEL: An angled part or surface; to slope at an angle.
斜面:与水平面成一定角度的平面。


BEVEL PROTRACTOR: A tool for measuring an angle or marking angles.
量角器:一种可以测量和标记角度的工具。


BILLET: An unfinished bar or circular of steel, or iron. The Timken Company seamless tubing is made from billets.
钢坯:未完成加工的钢棒或铁棒,用于生产Timken 公司的无缝钢管。


BIT: The biting, cutting or penetrating part of various tools; the moveable boring or drilling part used in a carpenters brace; a drilling machine. Anything that curbs or restrains. Also: A computer term which refers to the smallest possible unit of information utilized by the computer.

钻头:不同工具的尖锐的部位,用于钻孔,切削及打孔;木匠用的手拉曲柄钻的可移动的钻头;一种钻孔工具。任何限制或约束。也称比特,一个计算机术语,指计算机里的信息的最小单位。


BLANK: The circular piece of metal which has been cut from a flat piece of steel but which is not yet punched or perforated into a form nearing that of a completed cage.
毛坯:从方形钢块切割而来的尚未冲压成保持架形状的圆形金属块。


BLANKER: First stage of operation in cage department which forms the cage; forms steel to approximate outer diameter and height, also cuts unused portion of strip into short lengths for scrap removal.
下料:保持架制造部门生产保持架的第一道工序;把毛坯切割成和保持架近似的外径和高度,同时把无用的剩料切割成短碎片以便于清理。


BLUEPRINT: A mechanical drawing, detailed plan, or outline. Most common prints used in the Railroad Bearing Business are Tooling Prints, or Product Prints.
蓝图:一种机械图纸,详细的平面图或轮廓。在铁路轴承业务中大多数图纸为工装图或产品图。


BLUING / BLUE UP: Process of using blue dye to coat a surface of a master, gauge, or piece of product to check a flat, circular, or tapered surface. The results of the bluing process show surface irregularities and/or dimensional defects.
着色检查:使用蓝色染料涂在模具,量规或者产品表面以检查平面、圆面或者锥面的工序。其结果会反映出产品表面的不规则和/或尺寸误差。


BORE: The process of enlarging an existing hole with a rotating cutting tool.
镗孔:使用旋转式切削工具扩大孔的过程。

 

BORE SIZE: The inner diameter of a cone, which accommodates a shaft.
内径尺寸:轴承内圈的内孔直径,安装于轴上。


BRAD: A thin, wire nail; sometimes peened on one end.
曲头钉:一种细金属钉;有时候一端是平头的。


BRIDGE: The vertical portion of the cage that actually spaces each roller properly around the cone assembly.
横梁:保持架垂直的部分,沿着内圈滚道正确隔开每一个滚子。


BRINNEL HARDNESS TEST: An indentation test commonly used for soft steel and metals, which measures diameter of an indentation made by a steel ball under a given load.
硬度测试:一种针对软钢和软金属的压痕试验,给以一个钢球特定的负荷让其压迫金属,在金属表面产生压痕,测量压痕的直径可以知道金属的硬度。


BUPI WASHER: Special piece of equipment used to wash tooling and Unipac bearings.
BUPI 清洗器:一种特别的设备,用于清洗工装设备和Unipac 轴承。


BURN: A defective area caused by overheating during various grinding operations, usually causing discoloration or flat spots to the product. Some burns can only be determined by an acid test, some can be seen visually; they occur on front faces, back faces, ribs, outer diameters, and inner diameters. Also called Grind Burn Injury.
烧伤:在不同的磨削过程中由于过热而造成的缺陷,这种缺陷通常造成产品表面变色或者斑点。有些烧伤只能通过酸性测试来确定,有些则肉眼可分辨;烧伤产生在小端面、大端面、挡边、内圈表面或者外圈表面。也称为磨削烧伤。


BURNISH: To make shiny by rubbing; gloss, polish.
磨光:通过研磨,抛光的方法来增加表面光洁度。


BURR: A rough, raised piece or bit of metal; when a bearing is gouged it leaves raised areas of metal around the gouge which are referred to as burrs.
毛刺:指金属表面的粗糙的小金属突起;当轴承放进量规测量后,沿着量规的内表面会有轴承遗留下来的微小金属突起,这些小突起被称为毛刺。


BUTT END: The piece of steel tube left over after the last cup or cone has been cut in the screw machine operation. Most butt ends are returned to Canton to be melted and used again. In some cases they are saved for other manufacturing operations.
平头端:指冲切机冲切了最后一个内圈或外圈所剩下的钢管。大多数的平头端被送回Canton 熔化重新利用。在有些情况下它们被保存起来,用于其它的一些制造过程。

 

-----
返回顶部

-----


CAGE
: Spacer used to maintain proper roller distribution around cone in assembled bearing; holds unit together.

保持架:轴承组件中用于使滚子保持一定间隔分布在内圈滚道上的装置。


CAGE SCRAP: Scrap produced during the process of stamping out cages.
保持架废弃料:在生产冲压钢保持架过程中产生的废弃料。


CARBIDE: A very hard and brittle carbon compound molded to form cutting tools. Also used as wear strips in gauging devices such as reference stops and surface plates.
碳化钙(工具钢):一种坚硬且脆的碳化物,可制作切割工具。也可用在量具上刻记号。


CARBURIZING: The process of heating steel to a high temperature for a specific period of time while in contact with a material or gas which is high in carbon content. This forces carbon into the outer surface of the steel. Timken Bearing parts have a hard, wear resistant outer surface and a relatively soft, tough inner core.
渗碳:钢材热处理的一个工序,将钢材加热到高温并保持一段时间,期间让钢材与含碳量高的物质或气体接触。强制使碳元素进入钢材的表面。铁姆肯公司的轴承组件采用这样的热处理,使之拥有坚硬抗磨的表面和较软坚韧的内核。


CASE: The hardened, high carbon, outer surface of a piece of metal or steel.
表面高碳层:钢铁或金属的坚硬高碳表层。


CAVE: (See: Nib)
凹坑:(详见:Nib)


CHAMFER: The flat surface formed by cutting away the sharp edges of two meeting surfaces.
倒角:两个表面相交处,通过切掉尖锐边缘形成的平面。


CHAMFERING MACHINE: A machine which completes the green turning operation; it removes the sharp edges of cups and cones.
倒角机:用来完成车加工的机器;它可除去外圈和内圈的尖锐边缘。


CHATTER: Surface defect on a given piece of product; defect appears as a wavy pattern of lines.
波纹:产品表面的一种瑕疵;表现为波浪造型的曲线。


CHECKER: A Job Checker is an appointed Application Engineer within Product Management. This Application Engineer will check the quality, accuracy, and thoroughness of your work on an engineering job.
检验员:产品管理中任命的一个工程师。他的职责是检验产品的质量,精度和整个工程作业。


CHERRY RED: The term used to refer to a certain temperature range of hot product; cherry red process means observing hot product and guessing the temperature of product by its color.
樱桃红:用于表示高温产品的某个温度区间;樱桃红工序表示通过观察产品的颜色来猜测高温工件的温度。


CHIP: (See: Spall)
碎片:(详见:spall)

 

CHIPS: Scrap bits of metal which are removed during the screw machine operation and caused by metal turning operations; they are returned to Canton for reprocessing.
铁屑:在螺旋转动以及金属车削加工中产生的金属碎片。


CLOSE IN: A quality control process which selects cages by random sample and which temporarily assembles them into a complete bearing; purpose is to determine whether or not the assembled bearing meets proper specifications.
保持架压合:一个质量控制流程:随机抽选保持架然后临时装配成一个完整的轴承;目的是检验装配的轴承是否满足相应规格。


COCKING: Undesirable defect caused by blanks or cages not seated or aligned in dies properly.
歪卡:原坯或保持架没有恰当的放置在模具里而造成的未预料的瑕疵。


COLLET PAD: Part of a green machine which has serrated teeth and which holds the steel tubing in place during the green machining operation.
机床爪钳:车床上在车加工时固定钢管的齿形夹具。


COMPLETE CHANGE: The process of making changes necessary to produce a new part number series. Also referred to as a set up.
完全改装:因为生产不同的产品系列而需要对机床进行必要的工序改变。


CONCENTRIC: Circles or diameters which have identical centers.
同心的:圆周或者直径有相同的圆心。


CONE: One of four basic components of the assembled bearing; also referred to as the inner race. The bore of the cone accommodates the shaft, which runs through the bearing assembly.
内圈:轴承组件的四个基本组件之一;也可称内滚道。内圈内孔装配在运转的轴上。


CONTINUOUS PROCESS: A method of processing or production in which raw materials are continuously fed in and finished products continuously drawn off without interrupting operations. Many Timken bearing plants use continuous lines. (See: Batch Process )
流水线工作:产品生产的一种方法或工序:生产时,原材料不断进入生产线,成品不断下线。很多铁姆肯公司轴承生产厂都采用流水线生产。(详见:Batch Process)


CONTROL CHART: A graphical chart with upper and lower limits and plotted values of some statistical measure for a series of samples; used in the process of monitoring temperature, gas flows, and size control. (See: X-Bar Chart , R-Bar Chart )
控制图表:针对一系列样品的统计学图表,图上有指标的上限和下限以及样品的实际测量值;用于控制温度,气体流量,尺寸控制等的工序中。(详见:X-bar chart, R-Bar chart)


CONTROLLED CONTOUR: A profile following a designated pattern; cones that are dubbed or rounded into the undercut and recess of cone raceways; a profile following a designated pattern.
修形控制线:表面修形时参照的设计形式。内滚道上鼓起和倒圆时参照的设计形式。

 

CONTROLLED COOLING: Process by which steel is cooled from an elevated temperature in a predetermined manner to avoid excessive hardening, cracking or internal damage. A process to produce a desired microstructure or mechanical properties.
强制冷却:将高温钢材强制冷却到设计温度的工序,可防止钢材硬化过度,破裂或者内部损伤。是金属产生内部设计结构和机械性能的工序。


CONTROL LIMITS: Limits on a control chart, which is used as criteria for judging the significance of variations between samples or subgroups.
控制界限:控制图表上的界限,通常用作判断误差的标准。


COOLANT: Fluid used to remove heat from tooling and pieces of product as they pass through the manufacturing process.
冷却液:通过流经工装和产品时带走热量的液体。


CORE: The soft, ductile, low-carbon inner area of a hardened piece of product.
内核:渗碳产品内部的柔软的易延展的低碳的部分。


CORROSION: The destruction of a metal by chemical or electrochemical reaction with its environment.
腐蚀:因金属在环境中产生化学反应或电化学反应引起的金属破坏。


CRACK: Surface defect on product caused by improper heat treating process during the process of producing steel.
裂痕:因为热处理工艺不恰当而产生在产品表面的损伤。


CREW SHEET: Planning sheet which lists by name the employees assigned to a given work crew.
工作成员表:列出负责某任务团队所有员工名字的计划表。


CRIB: Unit used to store tooling; a storage system for jobs that have to be machined ground, inspected, etc.
储存区:用于储存工装的单元;用于储存未完成工件的系统。


CRITICAL TEMPERATURE: Temperature at which, upon heating, a steel transforms into the structure called Austenite. For most steels this occurs between 1350 degrees F. and 1500 degrees F.
临界温度:钢材加热使得内部结构产生奥氏体时的温度。通常大部分钢材的临界温度在华氏1350 度到1500 度之间。


CROWN: A convex surface on the raceway of a cone or the outer diameter of a roller. Degree of curvature cannot be determined by the naked eye.
凸弧:滚道表面或滚子表面突起的修形。曲率无法通过肉眼来分辨。


CUP: One of four basic components of the assembled bearing. Also referred to as the outer race; the cone assembly fits into the cup.
外圈:轴承组件的四个基本组件之一,也称作外滚道;内圈装配在外圈里。

 

CUTTING FLUID: Fluid applied to a cutting tool to assist the cutting operation by cooling, lubricating, or other means.
切削液:切削时用于降温,润滑等作用的液体。


CYCLE TIME: Amount of time product spends in a furnace at specified temperature for the purpose of carburizing or hardening product. Also total time for any machine to cycle through a series of operations.
周期:产品在炉中某特定温度下渗碳或硬化所需要的时间。也可以指任何机器完成一系列操作所用的总时间。

 

-----

返回顶部

-----


DAMAGED GREEN: Any defect on a piece of product which was caused during the green machining operation or prior to the time the product is hardened.
初加工缺陷:是指由于初加工造成或在产品热处理之前,产品存在的任何一种缺陷。


DAMAGED HARD: Any defect on a piece of product which was caused during the hardening process, or any damage occurring after green machining up to and during the hardening or carburizing process or at any time prior to the grinding operation.
硬化损伤:这种产品缺陷可存在于生产的各个阶段,可能是由于热处理造成,或是发生在从机加工到热处理的这段过程中,或是渗碳时造成的,也或是存在于磨加工之前。


DAMAGED OUTER DIAMETER: Any damage to outer diameter; can be caused by any of the manufacturing operations or by mishandling of the product.
外径缺陷:是指任何在外径上的缺陷,可能产生于制造过程,也可能源于误操作。


DATE CODE: One or more letters and numbers stamped on cups and cones to indicate the month and year they were produced. The Engineering Department provides the, letter date code, which is used instead of the customary numerical date system.
日期代码:由一个或多个字母数字组成,打印在内圈或外圈上,用以表示它们的生产年月。该代码由工程部门提供,用于取代常见的日期编号系统。


DE-BURR: Removal of sharp edges of product left by cutting tools.
去毛边:通过切削工具,去除产品的锐边。


DELAY TIME: The inadvertent delay in the manufacturing of product; production temporarily stopped.
延期:是指产品制造过程中的延迟,生产暂时停止。

 

DIE: Various tools or devices for stamping, cutting, or shaping.
模具:各种制造工具,用于冲压,切割或成型。


DIMENSIONAL INSPECTION: Method used to check product made by machines and then gauges using masters and dial indicators to check them in comparison to blueprint specifications.
尺寸检查:指各种检查产品的方法,采用标准零件进行比对测量,采用量表检查待检产品是否符合图纸的规格要求。


DISPATCH: Centralized radio communication center for the purpose of facilitating communicationamong all departments of The Timken Company.
Dispatch:集中式无线电通讯中心,用于方便铁姆肯公司所有部门之间的沟通。


DOG KNOTS: Steel left on perforated cage surfaces. Usually caused by excessive clearances on cutting surfaces, undesirable defect.
Dog knots:是指经过冲压后保持架上留下的余料,这是一种产品缺陷,通常是由于切割表面间隙过大造成的。


DOUBLE RECESS: Green roller defect of the large end recess caused by punch and head operations being misaligned.
双凹面:是指在热处理之前,圆锥滚动体大端凹处的缺陷,这是由于冲压大端时的跑偏造成的。


DRAG OUT: Defect on the inner diameter, outer diameter, or faces; undesirable spiral grind lines caused by too much pressure when the cutting tool or grinding wheel left the piece of product.
DRAG OUT:指那些由于切割工具或砂轮与零件之间过大的压力而留下的螺旋形磨痕,是一种存在于内径,外径或端面上的缺陷。


DROP HARDENING: The process of dropping small cups and cones and all rollers directly from the drop hardening furnace into an oil bath which quenches them.
DROP HARDENING:是指将小尺寸的外圈,内圈和所有滚动体直接从熔炉里抛到冷却油中进行淬火的工艺过程。


DROP WORK: Slang term for cups and cones which have been drop hardened.
DROP WORK:是指经过drop hardening 的外圈或内圈。


DUB OFF: Crown finish used to relieve pressure of the roller against the cone. (See: Crown)
DUB OFF:是指一种表面弧形处理,用于消减滚动体和滚道之间的压力。

 

-----

返回顶部

-----


EARS
: Excessive burr left at top corners of perforated cage; undesirable defect. (See: Burr)
EARS:指经过冲窗后,在保持架边角处的过多余料,这是一种表面缺陷。


ECCENTRIC: Circles or diameters not having the same exact centers.
偏心:是指各个圆或柱,其中心不在同一点上。


ECONOMIC LOT SIZE: Minimum order size which allows a break-even point between selling price and total manufacturing cost.
经济生产批量: 是指最小客户订单,以取得在销售价格和制造成本上的平衡点。


EFFECTIVELY MANAGING MAINTENANCE ACTIVITIES: Procedure for planning and executing all maintenance activities efficiently; procedure tracks, summarizes, and records those activities.
维修活动有效管理:是指各种有效地计划和执行维修活动的措施,包括了对维修活动的过程跟踪,总结和记录。

 

ELECTRONIC STATISTICAL PROCESS CONTROL: Timken Company developed software for PC based data collection and Statistical Process Control or SPC.
电子统计过程控制:这是一种由铁姆肯公司开发,基于计算机数据采集和统计过程控制的软件。


END OF PUN: Attention to a given amount of product has been completed in one department and is ready to be sent to the next department.
END OF PUN:是指对在一个生产环节已完成将要转移到下个生产环节的产品的关注。


EP LUBRICANT: Special extreme pressure lubricant which prevents metal to metal contact of mating parts and which imparts to rubbing surfaces the ability of carrying greater loads than would be possible with ordinary lubricants; prevents excessive wear or damage to parts.
极压润滑剂:一种特殊的极压润滑剂,可分离两接触物体间的金属表面,而且和普通润滑剂相比,它可使两摩擦表面之间承受更高的载荷,防止对产品造成额外的磨损和损坏。

 

-----

返回顶部

-----


FACE GRINDING
: Parallel grinding of the front face and back face of cups and cones; usually done on Gardner Grinders. Removal of stock from faces of cups and cones while maintaining size, parallelism.
端面磨加工:内外圈小端面和大端面平行磨加工;一般在加德纳(公司名)磨床上加工,在保证尺寸,平行度的基础上从内外圈端面把余量加工掉。


FERRITE: A room temperature structure of steel formed when slow cooled from above the critical temperature. Low in carbon and relatively soft.
铁素体:从高于临界点的温度缓慢冷却下来时形成的一种钢铁常温组织结构。


FINGER: As in perforator finger refers to perforator punch; as in carrier bar, refers to the jaws that pick up, carry, and release cages in next operation.
冲头/爪:在冲孔机里是指冲头;在搬运操作中是指抓起,搬运,松开保持架的爪。


FIRE POINT: The temperature to which a combustible liquid must be heated so that the released vapor will burn continuously when ignited under specific conditions.
燃点:在特定条件下引发后,使易燃液体可以释放出蒸汽并且使其持续燃烧的温度。


FLASH: Green roller defect, caused by excessive stock forced out between taper die and head die.
毛刺:过多余量从锥模和顶模中挤出后引起的软滚子缺陷。


FLAT ROLLERS: Undesirable rollers produced from scored wire.
刮纹滚子:刮伤的线材生产出来的不合格滚子。


FRACTURE TEST: A method of breaking sample product into pieces for test purposes.
断裂测试:出于试验目的而使样件断裂的一种方法。


FRICTION: Factor, which makes it difficult to slide one object over another, slows down motion and makes parts wear due to increase in temperature.
摩擦:使一物体在另一物体上滑动变得困难,降低运动速度,使温度升高而使零件磨损的因素。

 

FRONT FACE-CONE: Front face of a cone is at the small outer diameter end of the cone; the narrow end of a cone. The surface that is perpendicular to the inner diameter.
内圈小端面:内圈小端面是指内圈外径较小的一端;内圈较窄的一端,端面垂直于轴线的方向。

 

-----

返回顶部

-----


GAULDED ROLL
: Defect on the cage caused by punches, which do not move freely on the center pin; cause a deformed bottom or side of cage.
卷边:由于冲头不能在中心销上自由地运动,造成保持架底部或者边侧的变形缺陷。


GIB: A machine part, usually tapered, that is used on slides for adjustment purposes.
楔形块:一种安装在滑座上用以进行调整的机械零件,通常为锥形。


GONDOLA: Railroad car used to ship metal scrap.
运料车:用于运输金属废料的铁路货车。


GRAPHITE: A crystalline form of carbon having a laminar structure; of natural or synthetic origin.
石墨:一种由层状碳组成的结晶体,可以是天然的或者人工合成的。


GREASE: A lubricant of oil or oils thickened with a soap, soaps, or other thickener to a semi-solid or solid consistency. Conventionally, greases used by The Timken Company Bearing Operations are petroleum oils of some viscosity and thickened by soap.
油脂:一种由油、或含皂基成分而稠化的油、或含其他稠化剂形成的半固体状或固体润滑物。Timken公司轴承所用的油脂通常是含有皂基、带有一定粘度的石油类润滑脂。


GREEN: Product which has not yet been heat treated.
毛坯件:还没有进行热处理的产品。


GREEN CONTROL NUMBER: Numerical system, which is used in the scheduling of product to be green machined and carburized.
毛坯件控制号码:是产品进行毛坯加工和渗碳处理时所用到的号码系统。


GREEN MACHINE SCHEDULE: Daily, computerized schedule of tubing stock organized by outer diameter size, to be run on the screw machines per customer requirements.
毛坯件机加工计划:对按照外径分类好,按客户需求在车床上加工的管材的日常计算机管理计划。


GREEN MACHINING: The initial green machine operation which takes steel tubing and cuts it into cups or cones; the term green refers to turned product that has not yet been carburized nor hardened.
毛坯加工:对钢管进行切削加工成外圈或内圈的初始机加工;毛坯的定义是车加工成的产品但还没有进行渗碳或者硬化处理。


GRIND: Precise removal of stock from a given piece of product by way of grinding action.
磨削:通过磨削精密去除产品上的一些材料。

 

-----

返回顶部

-----


HARDENING
: Case hardening process whereby the carburized outer surface is made hard and strong while the center (core) is made tough and flexible.
淬火:是使渗碳的表面变硬,芯部变得有柔韧性的表面硬化工艺。


HARDENING CONTROL NUMBER: Numerical system used in the scheduling of product moving through the hardening operation.
淬火控制号码:用以安排产品进行淬火处理的数字系统。


HARDSTOCK: The rollers, cups, or cones, which have gone through the heat treat process and are ready for grinding.
硬坯:是已经过热处理的、准备磨加工的滚子、内圈或外圈。


HEADER MACHINE: Cold forging machine used to produce rollers.
镦头机:用于生产滚子的冷锻设备。


HEADER STOCK: Coils of wire which are cut and headed to form rollers. Header stock is also referred to as wire.
镦头原料:可通过切割和镦头工艺加工成滚子的金属线卷材。镦头原料也称为金属线材。


HEADING: The process of transforming wire stock (steel rods) into rollers by a cold forming operation which compresses a wire slug into a header die.
镦头加工:一种把金属线材(钢棒)的段头压进镦头模具而冷成型加工为滚子的工艺。


HEAD PULL: Green roller defect caused by improper machine timing; results in nick or indent of large end of radius.
端部撕扯:由于不正确的设备节奏而导致的在大端面处形成的凹刻痕状滚子毛坯缺陷。


HEAT TREAT: Process used on most alloy steels to provide desired metallurgical properties and to put them in the most suitable condition for machining or other subsequent operations. A combination of heating and cooling operations which create the desired ductility or case hardness desired in the product.
热处理:用于使大多数合金钢产生期望的金相组织特性并把这些组织处于为机加工或者后道工艺最适宜的状态的一种工艺。是使产品得到期望的延展性或表面硬化的冷热联合作用工艺。


HIGH SPEED HEADER: Newer type of cold forging machine which produces rollers at a faster rate than the old style machine.
高速镦头机:具有比旧式镦头机更快滚子加工速度的新型冷锻设备。


HOIST: An apparatus which exerts a force for the purpose of lifting or lowering.
起重机:一种通过施加一定的力来提升或放降物体的设备。


HONE: To smooth or finish; to polish. A process used to smooth a ground surface.
珩磨:对磨加工过的表面进一步进行抛光、磨光处理。

 

HONE NOT FINISHED: Defect on honed surface; finish ground surface not cleaned up adequately by the honing operation.
珩磨未完:珩磨表面的缺陷,磨加工过的表面通过珩磨工艺没有变得足够光洁。


HONER: Machine which uses honing tape to improve surface finish of cups, cones, and races.
珩磨机:用于对内圈、外圈和滚道进行珩磨来提高表面光洁度的设备。


HOOKS: Undesirable visual defect at large end of cage pocket. Protrudes out causing cage to cock when transferred from press station to next station. (See: Burr)
钩刺:在保持架窗孔大端面上的外观缺陷。当保持架从挤压状态转换到下一个状态时,突出物造成保持架翘起。(参见:Burr)


HOPPERS: Containers of many types used to store cups, cones, rollers, or cages.
储料器:可用于存放内圈、外圈、滚子或保持架的有多种类型的容器。


HYDRAULICS: The science dealing with water or other liquids in motion; its uses in engineering and all the laws governing its action.
流体力学:研究水或者其他流体运动的学科;该原理被用于工程中和所有控制规律研究。


HYDROMATION: A system for filtering and cleaning fluids previously used in machining operations.
滤清系统:在机加工工艺中被用于预先过滤和清洁液体的一个系统。

 

-----

返回顶部

-----


IN-PROCESS PRODUCT
: Product which exists somewhere between the beginning and final stages of completion.
半成品:介于原始材料和最终成品之间的产品。


INSPECTION: The process of checking product to make sure it is of excellent quality; can be done visually or by using gauges. That which can be done with the naked eye is called visual inspection; that which is done by gauges is called dimensional inspection.
检测:检查产品以保证好的质量的过程;可以使用工具来测或目测。肉眼检查的叫目测,使用检具来检查的工具检测。


INTERCHANGEABILITY: Bearing parts manufactured in one Timken Company Plant are interchangeable with those made in every other plant throughout the world.
互换性:在铁姆肯的一个工厂里生产的轴承零件可以和全球范围内的其他工厂生产出来的零件相互替换。


INVENTORY: An itemized list of capital; or given amounts of product.
库存:一个逐条列举的资产列表;或者特定数量的产品。


INVENTORY SHUTDOWN: One or two-week span of time at the completion of each fiscal year; reserved for the purpose of taking inventory for accounting purposes. Usually the last week of June and 1st week of July.
库存盘点:在每个财务年末的一周或两周,用于会计清算的目的,一般是六月的最后一周或七月的第一周。


IRON: A pure metal which serves as the basis for steel, cast iron, stainless steel, etc.; relatively weak and soft when in pure form.
:主要用作钢,铸铁,不锈钢等基本材质的纯金属,在纯质状态下比较软,强度较差。


ISIR: Initial Sample Inspection Report. This report is required by many automotive companies and some larger industrial accounts. This is their mechanism to assure them that the customer is supplying a quality product manufactured to spec. The customer usually requests this when they will use a new bearing for the first time. It also can occur when The Timken Company has significantly changed the process or design to manufacture the bearing.
初始样件报告:许多汽车客户和一些大的工业客户要求有这种报告。这是他们用来确认客户提供的产品是按照指定规格生产的。第一次使用一个新的轴承时客户一般要求这样的报告,或者当铁姆肯公司生产轴承工艺或设计有重大变化时也要提供这样的报告。

 

-----

返回顶部

-----


KNOCK DOWN: To disassemble a previously assembled bearing; the cage is cut or spread and discarded and the rollers and cones are salvaged and reprocessed.
拆卸:把已经组装好的轴承拆开;保持架被切掉或拆卸展开然后丢弃,而滚子和内圈从其取出并重新进行加工。

 

-----

返回顶部

-----


LAMINATED
: A strip steel condition appearing as a separation within the steel surfaces; an undesirable condition.
分层:条形钢材会出现的一种情况,钢材表面分层脱开;一般不希望出现一种情况。


LARGE INSIDE DIAMETER: The large end of the cup raceway.
外圈小端内径:外圈滚道面较大一端。


LOBE: High points on a given surface ranging from 3 to 7 as measured on a Lobe Gauge. (See: Chatter)
凸缘:在所检测的表面上凸缘检具测量值为3 到7 的高点。


LOT: A group of units (bearing parts) used for convenience in scheduling or material handling.
批次:为方便计划或处理而划分的一组轴承零件。


LOTS TO CLEAN: Metal pallets of 12 pans each, which are waiting to be shot blasted.
批次清洗:一次清洗12 个,等着进行喷丸。

 

-----

返回顶部

-----


MAGNA GLOW
: Process used to detect very small cracks; uses magnetic particles and inspection under an ultraviolet light.
辉光检测:用于检测非常小的裂纹的方法;使用磁粉在紫外线照射下检测。


MAINTENANCE ACTIVITY CARD: Card used in the management of maintenance activities. (See: EMMA)
维护保养卡片:用于维护保养管理的卡片


MENDER: The acronym MENDER stands for:
MENDER: 每个字母代表的含义为:


MEASURE - PHYSICAL ITEMS
测量 – 实物

EVALUATE - RESULTS SCIENTIFICALLY
评估 – 结果

NEEDS - IDENTIFY AND RECORD
需求 – 鉴别和记录

DEVELOP - ACTION PLAN
制定 – 行动计划

EXPENSES - CONSIDERED AND APPROVED
费用开支 – 考虑过并被批准的

REPORTING – RESULTS
汇报 – 结果


MENDER is a predictive maintenance program that is designed to define a machine's condition and recommend the action required to correct any faults in order to reduce machine downtime for mechanical delays.
MENDER 是一种预测性的维护保养方法,用于跟踪监测机器的状况,并采取必要的行动来改正存在的错误以此降低机器停工的时间。


METALURGICAL SAMPLE: A sample slug, part, or section of a carbonized, or hardened steel used for testing to determine structure, hardness, case depth, etc.
金相组织样件:渗过碳的或硬化处理过的钢材切片或零件,用于检测组织结构,硬度,渗碳层深度等。


MICROINCH: A unit of measurement for surface finish; measured in millionths of an inch.
微英寸:表面粗糙度的一种单位,一英寸的百万分之一。


MICROMETER: Instrument used to measure various distances, angles, etc.
千分尺:用来测量不同长度,角度等的工具。


MICROSTRUCTORE: The fine, internal structure of steel resulting from being heated to a critical temperature then quickly quenched. The microstructure, or how the parts that make up steel are arranged, controls how the bearing will perform.

微观组织结构:钢材被加热到临界温度以上然后迅速淬火形成的微观内部组织结构,微观组织结构或者说钢材内部组织是如何排列的将决定轴承的性能。


MIL: One thousandth of an inch. The Mil is commonly used to describe the thickness of thin items such as trash bag, The 1Mil is the one that won't get you to the street and the 2Mil is the heavy weight.
千分之一英寸:一英寸的千分之一,通常用于描述薄壁物体的厚度比如垃圾袋来说,千分之一英寸厚的无法装运和人类似重量的物体,千分之二英寸厚的就可以装运很重的东西。


MULTICHECK GAUGE: Gauge which has the capability of measuring more than one dimension of a piece of product.
多功能检具:可以测量一个产品许多种尺寸的检具。

 

-----

返回顶部

-----


NEC
: NATIONAL ELECTRIC CODE, the standards concerning anything to do with electrical work.
NEC: 国家电气规范, 与电气相关的标准。


NIB: Green roller defect on the small end radius; caused by taper die failure. A sharp protrusion on the small end of the roller.
NIB: 由于圆锥模具缺陷造成的半成品滚子小端倒角缺陷, 滚子小端有尖锐的突出。


NITAL ETCH: Process of checking surfaces of ground product for cracks or burns by use of a series of acids and neutralizers.
硝酸酒精腐蚀检验:通过使用一系列的酸性或中性溶液检查磨削后零部件表面是否有裂痕或磨削烧伤。


NOISE DOSIMETER: Instrument used to measure in decibels the amount of noise an employee is exposed to over an eight hour work day.
噪音测量装置:用于八小时工作小时之外测量噪音分贝量的仪器。


NO GO: Indicates that an order for product has not been satisfied; the term may imply a rush on the order because the customer needs have not vet been met.
不通过:表明一个产品的订单没有满足;该名词可意味着由于客户要求还不满足的条件下的匆忙订单。


NO STOCK: Surface of any piece of product which does not have enough stock to grind off in order to grind it to the correct size; usually visible as black, irregular area below abrasive contact.
无余量:任何零件得表面没有足够的原料可磨削至正确的尺寸,通常为黑色,不规则的表面低于研磨料的接触。


NO STOCK ID: Defect on inner diameter; large NCU condition indicating lack of stock for regrinding within specifications, machined undersize in green operation or caused by error in hardening process.
内孔无余量:内孔缺陷,大的NCU 条件意味着没有足够的材料磨削至技术要求,初加工尺寸过小或由于淬火过程的误差。


NOT CLEANED UP: Defect found on any surface of a piece of product; the rib or other surface did not clean up adequately during the grinding operation. Also called no stock. (See: No Stock )

不完全加工:零件任何一个表面的缺陷;挡边或其他表面磨削过程中没有完全完成工艺需要。


NOT TO MAN: Scrap produced by an operator which is not charged to him.
非人因素废品: 操作工生产的废品,但不算此人的废品率。


NOT TO PRINT: Product or machinery which is not made to concur with blueprint specifications.
未据图纸产品:产品或机器没有按照原始图纸要求生产。


NPM: New Product to Manufacture, is a system used for production. It replaced part number tooling data release (PNTDR) system.
新产品制造:新产品制造是应用于生产的一套系统. 新产品制造代替了型号工装数据分配系统。


NPR: New Product Request; system to obtain management approval, feasibility to manufacture product and obtain price of the product. New product request must precede other systems, such as SPO, NPM and POR.
新产品申请:新产品申请是为得到管理层批准的一套系统,该系统分析加工新产品的可能性,并获得新产品的价格. 新产品申请必须要在如SPO, NPM&POR 之前提出。

 

-----

返回顶部

-----


ON TIME DELIVERY
: A measure of pieces delivered to a customer within a given period vs. the expected pieces to be delivered. The customer can be internal or it can be the actual customer receiving the product. This is expressed as a percent and the actual method of determining delivery can vary by area.
准时交货率:评估产品在给定期限内交货给客户的情况与要求交货量的比较. 客户可以是内部客户也可是实际需要产品的客户. 这是以百分比表示,实际方法可以根据区域不同而不同。


OPERATIONAL SCRAP: Work that is scrapped prior to completing all operations on a line.
工序废品:没有完成产品线所有工序前的废品。


OTD: (See: On Time Delivery )
OTD:见准时交货率


OUT OF ROUND: Product that is elliptical (egg-shaped) and having its maximum diameter 90 degrees from the smallest diameter.
不圆:产品是椭圆形(蛋形)从最大直径处到最小直径相差90 度。


OUT OF TOLERANCE: Product which is produced outside of the blueprint specifications; product that is either below minimum or above maximum values assigned.
公差超差:产品没有按照图纸要求生产, 产品要么是过小要么是过大。


OEE: Overall Equipment Effectiveness, a measure of actual pieces produced for some period vs. the pieces possible for the same period expressed as a percent.
整体设备效能:以百分比评估表示的特定时间里实际生产零件与可能生产零件数的比值。

 

-----

返回顶部

-----


PEANUT
: Small sized pieces of product. Also called peanut product.
花生:小尺寸的产品,也叫花生产品。


PERFORATOR: Fourth stage of operation in the cage department. Simultaneously cuts out all pockets required in blank, maintaining proper top dimensions.
穿孔:在保持架部门的第四步工序. 同时按要求在切出保持架兜孔,维持合适的尺寸。


PIECEWORK: Incentive pay plan expressed in pieces.
计件生产:计件生产奖励机制。


PIERCER: Second stage of operation in the cage department; removes the bottom stock from the blank to the approximate inner diameter of the finished cage.
冲孔:保持架部门第二步工序,去除保持架兜孔底部的材料,其内径尺寸接近成品内径。


PIPING: A strip steel condition appearing as an overlap on the steel surface; this is an undesirable defect.
缩孔:带钢的表面有交错,这是不希望的缺陷。


PIT: 1) A reservoir that holds cutting solution in green machining operation. 2) Type of furnace used for heat treating bearing components.
PIT:1) 粗加工过程中切削液的贮备池。 2) 轴承零部件热处理炉。


PITTED: Small indentations appearing as black dots on finished surfaces of any piece of product; undesirable surface defects.
麻面:在任何成品零件的表面上出现的小的黑色的麻点,这是不希望的缺陷。


PLUG FURNACES: Retort, shaker, and hearth type hardening furnaces. (See: Plug Hardening )
塞式淬硬炉:蒸馏,振动器,锻造炉型的淬硬炉。


PLUG HARDENING: Process of maintaining proper size of larger cups and cones during the heat treat and quenching processes; sizing plugs are inserted into each piece of product during quenching.
塞式淬硬:在热处理&淬火过程中保持大尺寸内外圈尺寸的工序;在淬火过程中尺寸芯棒要塞入每个零件孔中。


PLUGS: Tooling used to insert into the inner diameter of larger size cups and cones to hold the correct size during the quenching process.
芯棒:用于塞入大尺寸内外圈孔中的芯棒,用来在淬硬过程中保持住正确的尺寸。


PLUS OR MINUS: Areas to the left or right of "0" on an indicator used to measure stock or a given dimension; larger or smaller than a given size.
正或负:计量仪表上”0”位的左边或右边,来测量给定的尺寸;比既定尺寸大或小。


POCKET: Holes in the cage which hold the rollers; Also refers to the large end recess of the roller. Also that portion of the taper die which forms the body of the roller.
窗孔:保持架上的用来保持滚子的孔;也用来指滚子大端面凹陷,也可指圆锥模具中成形滚子的部分。


POR: Prototype Order Request, a system to obtain prototype bearings.
POR:申请样品订单, 申请获得样品轴承的系统。


PROFILE: The true picture of a surface in relation to a horizontal line; a contour of a designated surface of a cup, cone, or roller.
型面轮廓:与水平线相比表面的实际轮廓线;实际设计的外圈,内圈或滚子的轮廓线。


PROFILOMETER: A compact, direct reading electronic instrument for measuring the height of surface roughness in microinches (millionths of an inch).
轮廓测定仪:小型的以微英寸(百万分之英寸)表示的直接测量表面粗糙高度的仪器。


PUNCH BOTTOM: (See: Piercer)
底部冲孔:(见冲孔)

 

-----

返回顶部

-----


QUENCH CRACKS
: Cracks formed in a steel part during or after quench, resulting from high stresses in cooling; could be caused by water in the quench oil.
淬火裂纹:裂纹在钢材的淬火或淬火后形成,由于冷却时的高应力所造成;也有可能是在淬火油中的水所导致。


QUENCHING: The process of rapid cooling from an elevated temperature. The product is placed in contact with liquids or gases, usually oil, water, or air.
淬火:指从某一高温快速冷却的过程。产品被放置于液体或气体中接触,通常是油,水或者空气。


QUILL: Cut off die.
套筒:切边模

 

-----

返回顶部

-----


R-BAR CHART
: A chart that charts and monitors the variation or spread of a statistical population, used in statistical process control.
R 型柱状图:制图并监测统计人口的变化和分布情况的图表,常用于统计过程控制。


R-DOUBLE BAR: The average of the R-Bars, used in statistical process control.
双R 型柱:R 型柱状图的平均值,用于统计过程控制。


RACEWAY: Also called a race; the tapered surface of either a cup or cone. The surface against which rollers revolve.
滚道:英语中也称race;指内圈或外圈的圆锥表面。该表面与滚子滚动接触。


RADIAL LOAD: The load that is caused by forces seeking to tilt, bend, or shove a shaft out of line. (See: Thrust Load )
径向载荷:该载荷是由轴的倾斜、弯曲、挤压或偏心所造成(参见:轴向载荷)。


RADIAL FORCE: The load on a bearing perpendicular to the axle, this and the Thrust load are forces that affect the design and application of bearings.
径向力:与轴承的轴线所垂直的载荷;它和轴向力是影响轴承设计和应用的两个力。


RECHAMFER: Defect on radii and chamfer; defective chamfer such as nicks that are considered to be repairable.
重新倒角:可被重新修复的倒角缺陷,例如划痕。


RED PAN: Pan of product at each screw machine; painted red to indicate that it is scrap. Red pan product is returned to Canton for reprocessing.
红盘:在车丝机上铁盘里的产品,涂抹红色表示它是废料。红盘产品需要被返送到坎顿回收再生。


RE-RADIUS: Denotes the need to correct defective radii on product such as nicked, torn, or undersized radii.
重新倒角:指需要修复产品上有缺陷的倒角,例如划痕,磨损或超差的倒角。


REPAIR: Product that is either visually or dimensionally out of tolerance but which can be repaired.
修复:能被肉眼观察到的或尺寸超差但能被修复的产品。


RIB: The cone has a rib at each and of the raceway. Ribs are at each end of the rollers when the bearing is assembled. Each cone has a large rib and a small rib which help position the rollers and keep the assembly from coming apart once the cage is closed in. (See: Unit Bearing )
挡边:内圈在滚道的两端各有一个挡边。挡边就位于组装轴承滚子的两端。每个内圈有一个大挡边和一个小挡边来定位滚子,并且在保持架封装后能防止装配件分离(参加:轴承单元)。


RIB STOCK: Extra steel left on green product to be ground during the finish grind operation.
边角料:在抛光研磨的操作中,从毛胚件上被去除的多余钢材。


RING: To tap an item; to check for cracks; the testing of a grinding wheel.
测试圆环:利用它来轻敲砂轮某一部分来检查裂纹,一种测试砂轮的方法。


ROCKWELL HARDNESS: An indentation hardness test which measures hardness by determining thedepth of penetration of a steel ball or diamond sphero-conical penetrator into the piece to be checked.The hardness number is related to the depth of indentation; the greater the number the harder thematerial.
洛式硬度:一种凹痕硬度测试,通过测量钢球或球锥形金刚石在所测工件上压入的深度来测定硬度。硬度的数值与压入的深度有关,该数值越大材料的硬度也越大。


ROLL: To reduce the size and change the shape of steel by squeezing it between large steel cylinders in a rolling mill. Most rolling operations are performed on hot metal but there are also cold rolling operations.
轧辗:为了减小钢材尺寸或改变其形状而采取的在轧钢厂通过两个大型的钢柱来挤压的过程。大部分的轧辗作业都用于加热的金属,但也有采用冷轧的方式。


ROLLER: One of four basic components of an assembled bearing. The roller is tapered, has a somewhat spherical shape and when assembled fits against the large rib of the cone. The rollers roll freely between the cup and the cone.
滚子:轴承的四种基本元件之一。圆锥滚子在和内圈大挡边接触的地方有一个稍带球面的形状。滚子能在内圈和外圈间自由的滚动。


ROLLER SIZE REPORT: Daily computer printout sent from Canton to Columbus; reports roller part numbers by class (honed or surface).
滚子尺寸报告:每天计算机打印出的报告由坎顿送往哥伦巴斯,通过分等级(精磨或超精磨)的滚子部件号来报告。


ROUGH HONE: Grinding.
粗磨:磨加工的一种


RUN ALL STEEL AT MACHINE: Instruction from supervisor to operator to use up all available steel at machine.
使用完机器内所有(钢)材料:主管对操作员的一个指示,用完所有在机器内可被利用的(钢)材料。


RUN ALL STEEL IN YARD: Instruction from Production Planning Department to supervisors and stock checkers to use up all tubing and steel stored in the yard or storage area.
使用完所场地内所有钢材:由生产计划部门向主管和库存检查员传达的指示,用完所有在该场地内或库存区的钢管或钢材。


RUN OUT: An undesirable condition that exist when the products outside diameter and inside diameter is not concentric. (See: Out of Round )
跳动:一种产品外径和内径不同心的非期望状况(参见:圆度超差)。


RUN OUT STEEL: Instruction to green machine operator to complete a scheduled job, to finish cutting the bar (tubing) and then refrain from loading any more tubing on the machine.
(钢)材料耗尽:一种要求切削操作工完成规定工作的指示,完成所要切削的钢棒或钢管,避免机器内还有多余的钢管。


RUST: Type of defect found on any surface of, any piece of product which appears as stain or corrosion resulting from atmospheric conditions or handling.
生锈:一种在表面产生的缺陷,任何一件产品置于大气环境下或使用中都会导致锈斑或侵蚀的发生。

 

-----

返回顶部

-----


SAMPLE
: One or more pieces of product taken from a larger group of product for the purpose of judging the quality of the larger collection.
样件:为了判断一个批次或多批次产品的质量,从一批产品中抽出的1 个或多个用于进行检测的产品。


SAMPLE SIZE: Limited number of pieces of product that are pulled from a total group for the purpose of checking them for quality.
样件数量:为了检查一整批产品的质量,从这批产品中抽出的产品的数量。


SCALE: Oxidization of iron that forms on the surface of hot steel exposed to air or oxygen.
氧化皮:暴露在空气或氧气中的高温钢铁,在其表面所形成的氧化铁。


SCALLOPING: (See: Wavy)
波浪形:(参见: Wavy)


SCARF: Process of removing build-up of oil and dirt crust from wood block shop floors.
去污:去除工厂木制地板上油渍和污渍的过程。


SCORE: A flat surface mechanically cut into round header wire to identify that portion of wire to be metallurgically defective. This operation is done at the Gambrinus Roller Processing Plant.
纵切面:为检验金属丝的金相组织而将金属丝沿纵向切开所得到的切面。这是Gambrinus 滚子制造工厂所采用的工艺。


SCRAP: When product that is either visually or dimensionally out of tolerance and can not be repaired; product that does not conform to blueprint tolerances.
废品:目测不合格或尺寸超差并且无法修复的产品;无法达到图纸公差要求的产品。


SET UP: Typically, the process of changing the tooling on a production machine tool in order to produce a different bearing component part number.
设置:改变或更换生产设备上的工装模具以生产不同型号轴承零件的过程。


SHOE: Top and/or bottom castings used to hold tooling in place on machine tools or presses.
工装夹具:在机床或冲床中用于夹持加工件的上模和/或下模。


SHORT FEED: Product that was not cut to length on green machine.
进给不足:在车床上由于进给不足而造成长度缺陷的产品。


SHOULDER: Defect found on rib or outer diameter; a raised edge on rib face caused by grinding wheel; raised surface at either end of outer diameter raceway.
挡肩:外径或挡肩上发现的缺陷;挡肩上由于磨床砂轮所造成的突起;在外径滚道两端的突起。

 

SIZE GROUP CODE: (See: Size Group Commodity Code )
尺寸组别编码:(参见:Size Group Commodity Code)


SIZE GROUP COMMODITY CODE: System The Timken Company uses to classify thousands of different component part numbers; organizes them into manageable and identifiable groups or lot sizes for production forecasting, scheduling, and control. Also called Size Group Code.
产品尺寸组别编码:Timken 公司用于将成千上万的零件型号分类的系统,将成千上万的零件型号分到不同的容易管理以及容易区分的组别中,便于产品的预测,排产以及控制。另一个名称叫做尺寸组别编码。

 

SIZER: Third stage of operation in the cage department; size blanks uniformly to proper outer diameter length and inner diameter dimensions.
尺寸定型:保持架加工的第三步工序;将毛胚件加工到适当的长度和内径。


SKID: Wooden skids used to haul materials and supplies.
滑动垫木:用于托运材料和物品的滑动垫木。


SKIP LOT SAMPLING: The random inspection of incoming items purchased by The Timken Company which causes some lots to be sampled and others to be skipped.
跳跃式的产品抽样:对Timken 购买的产品进行的随机性检查,这种检查会造成一些产品被抽检而另一些被略过。


SLOPPY: Extreme limits of tolerance, usually outside.
超差:公差的极限值,通常在外径上发生。


SLUDGE: An insoluble material formed as a result of either deterioration reactions in an oil or by contamination of an oil, or both.
沉积物:由于润滑油的惰化反应或者油里含有杂质所形成的不溶解的物质。


SLUG: Portion of blank removed by perforator operation; small portion of a winged or spread cage cut out, caused by cocking; removed portion of blank at piercer operation. (See: Piercer, Cocking)
废料:冲孔工艺中从毛胚件上冲掉的部分;带边的保持架上被冲掉的小部分;冲底孔工艺中从工件上去除的部分。(参见:Piercer, Cocking)


SLUICE WAY: Trench under all screw machines, which carry chips and coolant to one of two pits.
回流槽:在车床底部的沟槽,用与引导车削废料和冷却液进入一个或两个废料桶。


SLUSHING OIL: Oil or grease-like material used on metals to form a protective coating against rust, corrosion, etc.
防锈油:涂在金属表面,形成保护层,防止金属生锈或腐蚀的油或者油脂类材料。


SMALL INSIDE DIAMETER: Small end of the cup raceway. (See: Raceway)
小端内径:外圈滚道小端面直径(参见:Raceway)


SOAKING: Prolonged heating of a metal at a selected temperature.
浸泡:在特定的温度下,延长对金属的加热时间。


SOFT PRODUCT: Product that has not been properly hardened due to some problem in the heat treat process.
软件:由于热处理工序中发生问题而没有被淬火的产品。


SPALL: Rupture beneath the surface of a bearing part, which develops into a crack which lengthens and branches until a surface chip results. The chip is called a spall.
剥落:轴承部件表面下的微小裂纹将导致裂缝并扩散到金属表面,最终造成金属脱落,称之为剥落。

 

SPINDLE HEAD: Part of a machine, which supports and drives the grinding wheel.
心轴顶端:设备的一部分,用于支撑和驱动磨削轮。


SPLINE SHAFT: Shaft that connects the stock reel carrier to the machine; type 2 5/8" Conomatic L.F.
花键轴:连接托盘卷轴架与设备的轴;如在2 5/8 英寸的Conomatic L.F.型机床上可见。


SPO: Special Product Orders, special instructions to manufacture special (not standard) bearings in production environment.
SPO:特殊产品定单的缩写,生产特殊产品时向生产部门所提供的特殊产品说明。


SPREADER: Sixth stage of operation in the cage department; enlarges bottom of cage pockets for roller and cone assembly.
延展:保持架加工的第六步工序;对滚针保持架来说,是扩大保持架窗口的底部。


STAND: Overall width of the assembled bearing; refers to the combination of sizes of the cone, outer diameter, cup, inner diameter, and roller.
座高:整套轴承的总宽度;参考内外圈尺寸,外径,内径以及滚子。


STEEL: A mixture of iron, carbon, and other elements which can be heat treated to have a range of desirable properties, notably strength, hardness, and durability.
:由生铁,碳以及其他成分共同组成的混合物,能够进行热处理并且有很好的特性,比如强度,硬度和耐久性。


STOCK: Term has a variety of definitions; see specific department for clarification.
库存,股票等:有多中含义;参见各部门的说明。


STOCK REEL: Support reel for cone tubing on 2 5/8" Conematic L.F. and also 4 1/2" Acme.
送料滚轮:在加工内圈的2 5/8 英寸Conematic L.F.型和4 1/2 英Acme 型机床中用于传输管材的送料滚轮。


STORE: Centralized location for storage of parts, tools, safety equipment, etc., in the Railroad and Bearing Plants. Requisitions must be filled out for each item 'purchased. Requisition designates department, machine, and reason for usage.
存放区:在铁路运输或者轴承工厂中,产品、工具以及安全设备等集中存放的区域。每一件物品必须填通知单,通知单的内容包括指定的部门,设备和用途。


STRIP: Flat rolled steel used in the forming of cages. Hot or cold rolled to specified thickness, slit to specified widths and wrapped into coils.
钢带:卷起来用于加工保持架的带型钢材。通过热轧或冷轧达到一定的厚度,然后切割成一定的宽度并卷成钢带卷。


STUCK PUNCH: Term used interchangeably with Gaulded Roll. (See: Gaulded Roll )
冲压卷边:与Gaulded Roll 同义。(参见Gaulded Roll)

 

-----

返回顶部

-----


TAIL
: As in wire tail. The end, or last few feet of a coil of wire.
尾部:在电线的末端或者一盘线圈的最后的几英尺。


TAPER: Any surface of any bearing part that is not the correct angle or not to print.
锥度:任何轴承部件的表面角度不正确或者不符合图纸要求。


TAPER GRIND: Grinding process which produces angled surfaces, may be intentional or unintentional depending on blueprint specifications.
锥度研磨:研磨锥度表面的工艺,很大程度上依赖于蓝图的设计规范。


TEAR DOWN: To dismantle a machine set up on a machine or the disassembly of a previously assembled bearing.
拆装:拆除或安装一个车床,或者分解一个先前已经组装的轴承。


TEMPER: Process of re-heating hardened steel to a temperature below critical temperature followed by a desired rate of cooling; reduces brittleness in hardened steel; removes internal strains caused by sudden cooling in the quench process, give steel greater ductility and toughness. Also called aging or tempering.
回火:将已经淬硬的钢材再加热到低于临界点以下的某一温度,保温一定时间然后根据要求冷却到一定温度的工艺;减低淬火钢材的脆性;消除淬火留下的内应力;提高钢材的柔韧性。也被称为回火时效。


TENTH: Timken Company Slang for .0001 or 1/10,000; derived from the usage of measuring devices such as micrometers and mechanical indicators with discriminations of One Thousandth or One Ten Thousandth which became in shop terms Thousandths or Tenth Indicators.
万分之一:铁姆肯公司对.0001 or 1/10,000 称谓的内部行话。


THRUST LOAD: The load caused by forces seeking to thrush a shaft lengthwise. (See: Radial Load )
轴向载荷:由于轴在纵向受力所产生的载荷。(参考:径向载荷)


TIGHT IN CENTER: Condition of inner diameter of cone; inner diameter is not straight.
中心偏紧:出现在内圈的内径里,内径不是直的。


TOLERANCE: An allowable variation in the dimensions of a mechanical part; a minimum and maximum value assigned for the product to function properly; the product limits (plus or minus) as allowed by blueprint specifications.
公差:在机械部件里所允许的尺寸偏差量范围;为保证产品功能所设定了一个最小值和最大值;产品尺寸(加或减)受图纸规范的要求。


TOOL AND GAUGE INSPECTION: The metrology lab or standards department. The Tool and Gauge Department is the Timken Company link to the NIST - National Institute of Standards and Technology. Using proper measuring techniques and calibrated measuring systems, our masters, gauges and gauging devices are linked to NIST through NIST certified gauge Blocks and devices certified byappropriate venders.
模具和量规检测:计量室或者标准化部门。模具和量规部门是铁姆肯公司和NIST—国家标准和技术协会的纽带。使用恰当的测量技术和校对系统,我们的技术专家、量规和量具都是通过NIST 认证的。


TOPS: Refers to thickness of steel left at upper end of pocket, measured in height. (See: Pocket)
顶端厚:涉及到保持架窗口在上端部所留钢铁的厚度,以高度计量。(参考:窗孔)


TUBING: Seamless steel tubing used to make cups and cones, etc.; produced by The Timken Company.
钢管: 无缝钢管用来制造轴承外圈和内圈等,铁姆肯生产。


TUMBLERS: Cleaning units used to clean oxidized scale from rollers.
滚光清壳机:用来清洗滚子外层氧化物质。

 

-----

返回顶部

-----


UNDERCUT
: Tool used to cut away steel of the cone; leaves a void which is also called an undercut, at the roll race and rib intersection of the cone to assist the grinding operation.
底切(根切,退刀槽):切削轴承内圈的工具;在内圈滚道和挡边交接处为了磨加工所留下的空隙也叫做根切。


UNIPAC: A pre-assembled, pre-lubricated, bolt-on Timken unit bearing assembly designed for front wheel automotive applications.
UNIPAC 轴承单元:是一种预组装、预先调定游隙、预先润滑的汽车轮端轴承单元。


UNIT BEARING: An automotive bearing used that is sold as an assembled set and is non-adjustable; characterized by a cone with no large rib.
组合轴承单元:是一个应用于汽车上,在销售前预组装、无需调整游隙以及内圈没有大挡边的轴承单元。

 

-----

返回顶部

-----


VISUAL INSPECTION
: The examination of product against a known visual standard.
目检:根据视觉可见的标准来检测产品。

 

-----

返回顶部

-----


WAVY
: Strip steel condition causing top rim to be visually uneven. (See: Scalloping)
波浪状:带状钢条在顶部出现视觉可见的不平整。


WHISKERS: Slivers of steel left at top rim, or bottom of cage pocket, on cage; a undesirable defect.
金属须:留在保持架窗口上面或者边缘的金属丝,一种不合理的缺陷。


WINGER: The fifth stage of operation on a cage press that forms angle on bridges for proper roller angle, roller projection, and proper pocket length for finished cages.

边翼加工:在成品保持架横梁上冲压成型角度的第五道工序,来满足合适滚子角度、滚子注入和合适
的窗口长度。


WIRE: Round steel stock used in the production of rollers; cold drawn to a specified diameter and wound
in the form of coils.
钢丝:生产滚子用的圆形钢盘,冷拔加工特定直径并且卷成盘状。


WORKHEAD: Part of a machine that helps position, hold, and drive the rotation of the product.
爪盘:车床上用来帮助定位、夹持以及驱动转动产品的部分。

 

-----

返回顶部

-----


X-BAR CHART
: A chart that plots and monitors the centering of a statistical population. Part of statistical
process control.
x-柱状图:是一个用来划分和监控统计数据的一个图标。是统计工艺控制的一部分。


X DOUBLE BAR: The average of the X-Bar data.
双柱状:X-柱状数据的平均值。

 

-----

返回顶部

-----


YELLOW PAN
: (See: Operational Scrap )
黄色废料盒:(参考:生产中的废料)