Timken discusses the installation of two-row tapered roller bearings in wind turbines.
Two-row tapered roller bearings are increasingly preferred for managing dynamic loads in wind turbine gearboxes. Kyle Smith, a principal application engineer for Timken, penned an article discussing why it is critical to control the associated mounted setting for these bearings as they’re installed or replaced. Learn how component spacers work by reading Windpower Engineering & Development.
February 21, 2020