Timken Products Selected for High-Capacity Facility in Poland 

 

The Timken Advantage

High-capacity steel mills require high-quality parts to keep production up and running. With a global reputation for quality, Timken was recently selected by Siemens Metals Technologies in Austria as the exclusive supplier of tapered, spherical and cylindrical roller bearings for Arcelor Mittal’s new high-capacity hot-strip steel rolling mill in Krakow, Poland. Timken received the $2 million contract from Siemens, which is building the mill.
 
Timken bearings have been installed in various locations throughout the mill including the roll stands that shape the steel, cutting shears and the power coilers that wind the finished steel sheets onto a roll and other equipment. The mill was commissioned in the third quarter of 2007.

 

“Steel mill builders turn to us because we not only deliver product that improves a mill’s performance,” says Michael J. Connors, Timken’s vice president – industrial equipment, “but also because we work closely with builders to bring our first-hand knowledge of rolling-mill manufacturing to the design and selection of the bearing products for such a mill.”

 

With a steel strip width of up to 2100 mm, or 84 inches, the mill produces some of the widest finished products in Europe for carbon, stainless and special-steel grades to meet the higher quality needs of the automotive, petroleum and fuel industries. The new mill will also significantly reduce operating costs for Arcelor Mittal, while producing 2.4 million tons of steel annually, which is approximately 20 percent of total steel production in Poland.

 

Luxembourg-based Arcelor Mittal, the world’s largest steelmaker, invested around 300 million euros, or about $400 million USD, in construction of the Krakow mill. Constructed as part of a comprehensive modernization program, the mill is the first hot-rolled facility to be built in Europe in 10 years.

 

Siemens Metals Technologies (MT), a division of the Siemens Industrial Solutions and Services (I&S) Group, is one of the world’s leading engineering and plant-building companies for the iron and steel industry as well as for the flat-rolling sector of the aluminum industry and for open-cast mining. MT, which was created from the integration of Voest-Alpine Industrieanlagenbau, Linz/Austria, plus the electrical engineering product business and automation solutions of Siemens, provides a comprehensive range of supplies and services for all related technological processes and integrated automation solutions for the entire life-cycle of metallurgical plants.