Product List 

With more than 1.5 million tons of annual melt capacity, Timken produces one of the widest ranges of specialty steels in the world. Most of that steel leaves the Timken steelmaking facilities in the form of alloy and carbon solid bars or billets. In addition, much steel is produced as seamless mechanical tubing that is used in both our own bearing plants and also by our customers. Some of Timken steel is converted into value-added precision components such as blanks, rings and semi-finished parts ready for our customers to machine and process.

 

Hot-rolled alloy steel produced as solid bars and billets.

Seamless mechanical tubing produced from Timken® steel uses a rotary forging process that works the metal from both the inside and outside.

Value-added production processes convert Timken® steel into components with varying levels of value additions, from simple cut rings to near-finished parts.

Timken Boring Specialties, LLC combines leading well boring and finishing products with a wide range of Timken® high-quality alloy steel bars and tubes, resulting in a one-stop steel source for customers in the energy market.

Timken uses a combination of materials science, application engineering and processing capabilities to produce more than 300 types of steel.

A list of common steel grades for carburizing, through-hardening and induction hardening.


Steel Inquiries
Call us at:
1-866-284-6536
(Within the USA)
+44(0) 1530-512680
(From outside the USA)


Use Timken Direct
to check product availability or order status.
(username and password required)


Email us to request more information.

 

Related Links

 


Downloads

Practical Data for Metallurgists

Seamless Steel Tubing Overview

Special Bar Quality Overview

Small Bar Mill Overview

Large Diameter Tubing Overview

Value-Added Solutions Overview