CANTON, Ohio: Jan. 21, 2009 — The Timken Company (NYSE:TKR) today announced that it is supplying hot-rolled steel bars to Frisa Aerospace, a manufacturer of seamless rolled rings for applications in the aerospace, chemical and energy industries.
Based in Monterrey, Mexico, Frisa machines the 6-, 8- and 10.5-inch Timken® steel bars into mandrels. Mandrels are used to shape the rolled rings as they are being hot rolled and as a result need to be manufactured from high-quality grade steel produced by Timken. Timken supplies the steel bars to Frisa direct from its local warehouse and distribution center in Mexico. The distribution center, located near Mexico City, serves a wide range of original equipment manufacturers (OEMs), distributors and aftermarket customers in the Mexican automotive, industrial and steel markets.
About The Timken Company
The Timken Company (NYSE: TKR, www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers to perform faster and more efficiently. With sales of $5.2 billion in 2007, operations in 27 countries and approximately 25,000 employees, Timken is Where You Turn™ for better performance.
Source: The Timken Company
Media Contact: Lorrie Paul Crum
Manager - Global Media and Strategic Communications
Mail Code: GNW-37
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-3514
Facsimile: (330) 471-7032
lorrie.crum@timken.com
Investor Contact: Steve Tschiegg
Director - Capital Markets and Investor Relations
Mail Code: GNE-26
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-7446
Facsimile: (330) 471-2797
steve.tschiegg@timken.com
For Additional Information:
www.timken.com/media
www.timken.com/investors