12/18/2007 

 Timken Sensor Helps Crop Farmers Reap More Efficiency 

 

Chip Embedded in Tractor's Steering Motor Provides Feedback on Direction, Speed


CANTON, Ohio, Dec 18, 2007 (BUSINESS WIRE) -- The Timken Company (NYSE: TKR) announced today that it is supplying an innovative sensor that, combined with other steering system components, enables hands-free operation of tractors designed for planting and spraying row crops.


The Timken-developed feedback sensor is embedded into an integrated circuit board. Intelligent Motion Systems, Inc. (IMS) uses the sensor in its design of a motor used in the tractor's steering mechanism. The sensors provide feedback on the motor shaft position, and, when integrated with other steering system components, can directly impact the tractor's ability to operate in a hands-free environment.

 

"We were looking for a feedback device to embed into our motor's circuit, and as an engineering company, we wanted to work with a company that not only had the competency, but also was dedicated to the program," said IMS President David Coutu. "Timken was able to deliver on both aspects, bringing their technical expertise, production capabilities and support together to develop a low-profile sensor solution. In fact, we're now working on the next-generation technology for the application."

 

For more than six years, Timken has produced high-resolution magnetic sensors for use in a multitude of applications, including mobile, construction, factory automation, machine tool, semiconductor and medical. The sensor system embedded on the chip integrates speed, direction and position feedback functionality into a compact package. This design provides the user with an efficient means to obtain critical control feedback from a location close to the motion in an electromechanical package.

 

"As a leader in providing innovative power transmission solutions, we continue to investigate and develop sensor alternatives that solve challenging customer applications," said Greg K. VanBuskirk, Timken's business development manager for motion control sensors. "Working with IMS, this tractor-guidance system can improve productivity and lower operating costs by reducing operator fatigue, fuel consumption and row overlap while planting or spraying."

 

For more information on motion control sensors, visit www.timken.com.

 

About Intelligent Motion Systems

 

Intelligent Motion Systems, Inc. is the innovation leader in motors, drives and controls. Based in Marlborough, Conn., IMS offers a full line of high-performance motion-control products and accessories that are compact, powerful and reliable. Its products are routinely used in applications demanding highly precise, controlled movement including: robotics, medical, assembly, semiconductor, packaging and engraving.

 

About The Timken Company

 

The Timken Company (NYSE: TKR, http://www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers to perform faster and more efficiently. With sales of $5.0 billion in 2006, operations in 26 countries and approximately 25,000 employees, Timken is Where You Turn(TM) for better performance.

 

SOURCE: The Timken Company

The Timken Company
Media:
Jeff Dafler, 330-471-3514
Manager - Global Media &
Government Relations
Facsimile: 330-471-7032
jeff.dafler@timken.com
or
Investor:
Steve Tschiegg, 330-471-7446
Manager - Investor Relations
Facsimile: 330-471-2797
steve.tschiegg@timken.com
or
For Additional Information:
www.timken.com/media
www.timken.com/investors