CANTON, Ohio — March 3, 2008 — Building on its extensive line of industrial lubricants, The Timken Company (NYSE: TKR) today announced the addition of several quality lubricant-delivery products, including grease guns, pumps and kits.
The new products will be introduced in the United States this month, and in Canada during the second quarter of 2008. The lubricant-delivery product line complements Timken’s ability to go beyond bearing technology and provide friction management solutions that meet maintenance needs.
“Proper lubrication is critical to machine performance and component longevity, and customers routinely turn to Timken for help in extending bearing life,” said David A. Pierman, manager of Timken’s lubricant and lubricant-delivery systems for the Distribution & Services group. “Adding these lubricant-delivery devices to our product portfolio furthers our customers’ ability to achieve maximum machinery operation. Now they can use a Timken grease gun to deliver genuine Timken grease to their Timken bearings.”
Research indicates that more than 50 percent of all bearing damage is related to inadequate or improper lubrication. These new lubricant-delivery products help advance Timken’s strategy to aggressively strengthen its channel presence by extending its product lines around the bearing.
The guns and pumps are high-quality maintenance products that help decrease both machinery downtime and operating costs. They include:
- Deluxe series lever-type grease gun with metal barrel
- 18-volt battery-powered grease gun
- Standard-duty, high-pressure 55:1 grease pump
- Heavy-duty, high-pressure 55:1 grease pump
Product specifics include:
- Deluxe series lever-type grease gun:
- Made of tough, high-pressure cast iron which makes it unique in comparison to common pot metal or other die cast heads;
- Engineered to be easy to load, deliver grease evenly and withstand the hardest working conditions.
- Battery-powered grease gun:
- Powerful 18-volt rechargeable battery to grease more machinery in less time;
- Packaged with an extra battery to further minimize down-time and reduce wait-time for battery recharge.
- Standard-duty, high-pressure 55:1 grease pump:
- Handles all types of grease, up to and including National Lubricant Grease Institute (NLGI) 2, directly from 35-pound, 120-pound and 400-pound grease containers;
- Designed for portable and stationery systems that include pipe lines, hose reels and control handles;
- Highly efficient double-action pump design assures even flow of fluid, low noise level and low air consumption with built-in exhaust mufflers.
- Heavy-duty, high-pressure 55:1 grease pump:
- Handles all types of grease, up to and including NLGI 3, directly form 120-pound and 400-pound grease containers;
- Designed for applications with long dispensing lines where low pressure would limit pump performance. It is also optimum for cold weather conditions and severe-duty operations;
- Double-acting priming piston requires fewer cycles and produces less wear, thus increasing the life of the pump.
- Kits:
- Available for both the grease guns and grease pumps for hassle-free installation and operation;
- Grease gun kits include Timken Premium All-Purpose Industrial Grease and accessories and replacement parts. Grease pump kits include mounting adapters, drum covers and connecting hose installation hook-up kits.
For more information on Timken’s line of lubricant-delivery products, contact your Timken salesperson or visit www.timken.com/products/lubrication.
The Timken Company (NYSE: TKR, www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers to perform faster and more efficiently. With sales of $5.2 billion in 2007, operations in 26 countries and approximately 25,000 employees, Timken is Where You Turn™ for better performance.
SOURCE: The Timken Company
Media Contact: Jeff Dafler
Manager – Global Media &
Government Relations
Mail Code: GNW-37
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-3514
Facsimile: (330) 471-7032
jeff.dafler@timken.com
Investor Contact: Steve Tschiegg
Manager – Investor Relations
Mail Code: GNE-26
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-7446
Facsimile: (330) 471-2797
steve.tschiegg@timken.com
For Additional Information:
www.timken.com/media
www.timken.com/investors