2/23/2009 

 Timken Expands Line of Heavy-Duty Wheel Seals and Tools 

 

Outrunner® products enhance Timken aftermarket portfolio


CANTON, Ohio: Feb. 23, 2009 — Dedicated to delivering increased uptime and reliability to the heavy-duty truck aftermarket, The Timken Company (NYSE:TKR) is expanding its line of wheel seals and installation tools for the heavy-duty truck aftermarket. 


The Outrunner® line of products, sourced from a leading manufacturer and sold under the Timken® brand, complements the company’s existing product line and offers a premium wheel seal designed to meet the performance demands of low-maintenance wheel ends.


“These seals offer a high-quality product that aligns well with our dedication to bringing customers solutions that reduce friction and maximize uptime to keep their trucks on the road,” said Tom Tecklenburg – director – automotive and heavy-duty aftermarket.  “Timken already offers a wide range of products to the aftermarket that help deliver optimum friction management, and these Outrunner products are another strong addition.”


Two designs of this seal are available from Timken, the Outrunner Standard and the Outrunner PH (Performance Hybrid). The design of both variations promotes ease of installation and reduction of friction. Other features include an interlock design that provides enhanced dust- and leak-prohibiting protection, which lengthens bearing uptime and extends maintenance intervals.


The Outrunner PH seal features a hybrid metal and rubber outside diameter that reduces installation problems associated with other types of seal designs. The improved installation is achieved because the rubber in the hybrid compensates for minor bore imperfections and helps eliminate seal misalignment.  With improved installation, end users can perform maintenance quicker and get trucks back on the road faster.


The Outrunner PH also utilizes an exclusionary interlock labyrinth seal design that lowers torque and heat generation to promote longer seal life and potential fuel economy.


Users of the Outrunner seals also can benefit from reduced inventory stocking as the seal lip material is compatible with mineral, synthetic and semi-fluid greases. 


To further increase the ease of installation for end users, Timken also offers seal installation tools, which are engineered for Outrunner to help position and properly seat the seals.


For more information about Timken’s full line of automotive aftermarket products, please visit www.Timken.com/automotive.


Outrunner® is a registered trademark of Freudenberg-NOK.


About The Timken Company
The Timken Company (NYSE: TKR, http://www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers' machinery to perform more efficiently and reliably. With sales of $5.7 billion in 2008, operations in 26 countries and approximately 25,000 employees, Timken is Where You Turn™ for better performance.

 

 

 

SOURCE: The Timken Company

 

Media Contact:  Lorrie Paul Crum
Manager - Global Media and Strategic Communications
Mail Code: GNW-37
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-3514
Facsimile: (330)  471-7032
lorrie.crum@timken.com

 

Investor Contact: Steve Tschiegg
Director - Capital Markets and Investor Relations
Mail Code: GNE-26
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Telephone: (330) 471-7446
Facsimile: (330) 471-2797
steve.tschiegg@timken.com

 

For Additional Information:
www.timken.com/media

www.timken.com/investors