CANTON, Ohio: Sept. 14, 2010 — The Timken Company (NYSE: TKR) has launched a new line of precision cylindrical roller bearings designed to maximize speed, precision and efficiency in high-demand machine tool applications.
Timken’s precision cylindrical roller bearings for screw drives feature a combination of axial cylindrical rollers and radial needle rollers. This unique configuration helps manage loads from multiple directions during high-speed operation.
The precision cylindrical roller bearings for rotary tables feature an integrated design, with an L-shaped inner ring, shaft washer, outer ring, two thrust roller cage assemblies and a radial full complement row. The result is an easy-to-install unit that can manage stresses from multiple directions, including axial, radial and moment loads.
"These bearings can take on higher loads and withstand additional abuse, helping operators squeeze more out of their machines," said Greg Vanbuskirk, industrial business development manager of Timken's health and positioning control business.
In applications such as rotary tables, grinding and milling operations, where rotational accuracy, consistency and rigidity are critical, both the original equipment manufacturer and distribution markets will find these bearings particularly suitable for machinery builds, rebuilds and design.
"Machine tools are subject to some of the toughest conditions," Vanbuskirk said.
"Our customers are looking for bearing solutions that are reliable, help optimize their operations and allow for maximum productivity. Our precision cylindrical roller bearings are ready for the challenge."
The offering includes a screw-drive bearing series of five designs (90 mm and 3.54 inches ID maximum) and the rotary table bearing series (460 mm and 18.1 inches ID maximum), allowing customers to meet their machine-tool bearing needs from one source.
"We now offer a broader line of friction management solutions, from bearings, seals and lubrication to reliability, engineering and maintenance support," Vanbuskirk said. "The addition of precision cylindrical roller bearings for machine tool screw drives and rotary tables allows us to offer our customers a more complete system approach for greater ease of operation and value added."
About The Timken Company
The Timken Company (NYSE: TKR, http://www.timken.com) keeps the world turning with innovative friction management and power transmission products and services, enabling our customers’ machinery to perform more efficiently and reliably. With sales of $3.1 billion in 2009, operations in 26 countries/territories and approximately 17,000 employees, Timken is Where You Turn® for better performance.
The Timken Company
Media Contact: Lorrie Paul Crum
Manager – Global Media and Strategic Communications
Mail Code: GNW-37
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Office: (330) 471-3514
Facsimile: (330) 471-7032
lorrie.crum@timken.com
Investor Contact: Steve Tschiegg
Director – Capital Markets and Investor Relations
Mail Code: GNE-26
1835 Dueber Avenue, S.W.
Canton, OH 44706 U.S.A.
Office: (330) 471-7446
Facsimile: (330) 471-2797
steve.tschiegg@timken.com
For Additional Information:
www.timken.com/media
www.timken.com/investors