12/1/2010 

 Massive Boring Machines Rely on Timken When Making Way for the World's Longest, Deepest Rail Tunnel 

 

 CANTON, Ohio (NYSE: TKR): Dec. 1, 2010 — On Oct. 15, 2010, Switzerland’s Gotthard base tunnel became a reality. At 2:17 p.m. Geneva Time that day, a boring machine in the east tunnel located 6 km (3.7 mi) south of Sedrun broke through the last meter of rock deep inside the Alpine range.  The colossal 57-km (35.4-mi) Gotthard railway tunnel is the world's longest, most deeply set passage of its kind. It took 15 years, 3,000 workers, €9.1 billion (US$12.7 billion) -- and thousands of bearings made by The Timken Company -- to complete. 


Four Herrenknecht Gripper tunnel boring machines completed the work, which excavated and secured two parallel, main-tunnel tubes of more than 85 km (52.8 mi), for a combined expanse of 114 km (70.8 mi).  Since 2003, the cutter assemblies in these machines required thousands of Timken® standard and P900 tapered roller bearings. Frequent bearing replacement helped the machinery manage grueling loads and difficult conditions while making the passageway through the mountains.


Timken's P900 bearings feature surface modifications to help address performance concerns associated with the mountain conditions such as marginal lubrication, a maintenance constraint caused by an overburden of rock of 2,500 m (8,202 ft).  Additionally, special race profiles in the P900 bearings help manage the higher loads and misalignment conditions, which pose particular engineering challenges for deep tunneling applications. 


"This is perhaps one of the most challenging applications for cutter-specified tapered roller bearings," said Steve Boyd, Timken principal application engineer, who assisted the cutter design.  "The rugged terrain required a cutting action that subjected the bearings to highly variable loads.  Leading up to the start of this massive project, our customer engineering group provided detailed modeling of the bearing loads to assist in optimizing the bearing design."


Supplying such a large quantity of bearings through the duration of the project was a challenge. "During the actual tunneling phase, our customer service and supply chain teams had to maintain delivery and service levels to avoid any work stoppage over the eight-year work period," said John O’Hearn, specialist, Timken Tunnel Boring Sales.


Herrenknecht’s best boring machine performance on this project was a record-breaking 56 m (184 ft) – at a 9.5 m (31 ft) diameter – in a 24-hour period.  The top monthly tunneling performance for Herrenknecht’s boring machines was 711 m (2,333 ft).  As they cut deep inside the mountain, grippers at the rear of the boring machines braced themselves with two gripper plates against the rock.  From there, hydraulic cylinders pushed the cutter heads into the tunnel face.  Rock chips that broke out between the 75 mm to 90 mm spaced concentric cutter tracks at the face were removed from the tunnel to the surface on a conveyor belt.


David Krauter, Herrenknecht cutter product manager based in Sumner, Wash., said, "The cutters are rated for a load capacity of 267 kilonewtons (approximately 60,000 lbs.).  Because of the severe and challenging environment, bearing reliability was of great importance."


The Gotthard base tunnel in Switzerland connects the north portal in Erstfeld (Canton Uri) with the south portal in Bodio (Canton Ticino) and consists of two side-by-side, single-track tubes that are connected every 325 m (1,066 ft) with 40 m (131 ft) galleries.  Projected to be operational by the end of 2017, officials expect the tunnel to markedly improve high-speed passenger and heavy-freight transport in Europe.  Travel time between Zurich and Milan, for example, would be reduced nearly an hour – from 3 hours and 40 minutes to 2 hours and 50 minutes.

 

About The Timken Company

 

The Timken Company (NYSE: TKR, http://www.timken.com) keeps the world turning with innovative friction management and power transmission products and services, enabling its customers’ machinery to perform more efficiently and reliably. With sales of $3.1 billion in 2009, operations in 27 countries/territories and approximately 17,000 employees, Timken is Where You Turn® for better performance.

 

About Herrenknecht Group

 

Herrenknecht AG is a technology and market leader in the area of mechanized tunneling systems. It achieved sales of €866 million in the year 2009 and has more than 3,100 employees around the world. With 65 subsidiaries and associated companies working in related fields in Germany and abroad, Herrenknecht is able to quickly provide, in a targeted way, a comprehensive range of services in close proximity to project sites and customers.



The Timken Company

 

Media Contact: Lorrie Paul Crum
Manager – Global Media Relations & Strategic Communications
Office: (330) 471-3514
Mobile: (330) 224-5021

lorrie.crum@timken.com


Herrenknecht Group: Achim Kühn
Head of Corporate Communications, Branding and Public Affairs
Telephone:  +49 (0) 7824 302-540
Fax:  +49 (0) 7824 302-473
pr@herrenknecht.com

 

For Additional Information:
www.timken.com/media

www.timken.com/investors